Motor_Factor (Velocity_Factor_Denominator)
| Index.Sub | 2013.2H |
| Data Type | Unsigned32 |
| Access | Read/Write |
| PDO Mappable | No |
| Unit | -- |
|
Range |
1 to 4294967295 |
| Default Value | 1 |
| Store Supported | Yes |
| Description |
This object defines the denominator of the ratio for velocity factor used to convert user-defined velocity unit to internal velocity unit and vice versa.
The internal velocity unit is Hz (Inc/s). |
|
Notes |
|